Industry Online Support
Technical Forum
9/17/2008 9:24 PM | |
Posts: 487 Rating: (45) |
Yes it is possible Check this link. It shows wiring diagram for 4, 3 & 2 wire sensors. Please note that the red lines show the wiring external to the module. http://support.automation.siemens.com/WW/view/en/14955836 Check the link below for some more helpful info http://support.automation.siemens.com/WW/view/en/22149157 |
Last edited by: JMJ at: 9/17/2008 9:29 PMLast edited by: JMJ at: 9/17/2008 9:24 PM |
|
9/17/2008 9:32 PM | |
Joined: 7/15/2008 Last visit: 1/23/2024 Posts: 382 Rating: (44) |
Hello , Please see link below. I hope it helps. I used the 4 wire 4-20mA on a Molding Press. http://support.automation.siemens.com/WW/view/en/22148598 |
9/19/2008 5:13 AM | |
Posts: 1064 Rating: (72) |
one thing to remember is that you have to set the module to 4 wire input to use the 2 wire or your reference will be wrong |
9/27/2008 3:29 PM | |
Joined: 1/17/2007 Last visit: 10/6/2020 Posts: 289 Rating: (3) |
Thank you all for clearing this isue for me. |