10/15/2014 9:45 AM | |
Joined: 2/8/2012 Last visit: 12/22/2014 Posts: 2347 Rating:
|
Use a timer with 1 hour. If have elapsed, a pulse to a counter, which counts up to 2000. |
10/15/2014 11:57 AM | |
Joined: 1/5/2011 Last visit: 12/11/2020 Posts: 806 Rating:
|
Dear Kayhan, you should use a retentive timer. Check out how to create a retentive timer in S7-300: How do you program a timer that retains the time value at STOP and counts on starting at the stored value? Check out following link for the timers that can be used: How can you measure the time? I suggest you use runtime meters if accuracy isn't that important. Those can count up to 32767 hours. Kind regards, Jens |
Last edited by: Jens_app at: 10/15/2014 12:00 PMKeep it simple and on-topic. |
|
10/15/2014 12:50 PM | |
Posts: 7 Rating:
|
Thank you Dear Jens_app, I download file P_FB115.zip but, I do not know that how to use it . Can you help me pleaese ? |
10/15/2014 1:24 PM | ||||||||||||||||||||||||||||
Joined: 1/5/2011 Last visit: 12/11/2020 Posts: 806 Rating:
|
Dear Kayhan, what do you mean? You cannot open the file? Or do you want some guidance on how to use this FB? If it's some guidance on how to use the function, you should first take a look at the table which describes how to parametrize the FB:
So you call this function block and connect it to an instance DB, then parametrize it according to your program requirements. Kind regards, Jens |
|||||||||||||||||||||||||||
Last edited by: Jens_app at: 10/15/2014 1:33 PMKeep it simple and on-topic. |
||||||||||||||||||||||||||||
10/15/2014 2:58 PM | |
Posts: 7 Rating:
|
Dear Jens_app I am so sorry, I can not open file. I added file. Can you help me ? Firstly I opened the program such as photo 1 then I click File>Retrieve, then I selected the file that you have posted such as photo 2 then I selected the s7proj to save photo 3 then photo 4 is comming I clicked ok but end photo is such as photo 5. Program is not opening because of seting languge is english Thanks. AttachmentYeni klasör.zip (22 Downloads) |
10/15/2014 3:25 PM | |
Joined: 1/5/2011 Last visit: 12/11/2020 Posts: 806 Rating:
|
Dear Kayhan, Check out following thread to resolve your language issue: Cannot open Step 7 project because of language Next try extracting the project to a known path (for example "C:\Project\") then open simatic manager -> in the top bar, go to File -> Open -> Press Browse... -> go to the path were you extracted the project -> select the project and press OK. Let me know how it worked out... Gr, Jens |
Last edited by: Jens_app at: 10/15/2014 3:29 PMKeep it simple and on-topic. |
|
10/15/2014 3:39 PM | |
Posts: 7 Rating:
|
Hello Dear Jens_app I have tried that you say , but there is same error such as photo. Must I set simatic manager Germany ? I am so sorry. |
10/15/2014 3:50 PM | |||||
Joined: 1/5/2011 Last visit: 12/11/2020 Posts: 806 Rating:
|
Dear Kayhan, I don't think thatisnecessary, mine is set in english and it works fine. I have only heard of this problem, but I haven't encountered it myself. I'd try following step:
Try this step and let me know how it went, if that doesn't solve your problem I advise you to create a support ticket. Kr, Jens |
||||
Keep it simple and on-topic. |
|||||
Follow us on