Industry Online Support
Technical Forum
12/29/2014 8:18 AM | |
Joined: 5/12/2006 Last visit: 4/23/2024 Posts: 22224 Rating: (2979)
|
Hello, 20005 is a SIMOTION Technilogocal Error an don't documented in the SINAMICS List Manual. The SIMOTION Alarms described here. The 20005 means that there is anything not ok with the device which is projected on the adress which is in the faultvalue of 20005. please also check the sinamics faults, normaly when the 20005 occurrs there are other faultsbefore in the drive which is assigned to this axis. Regards Christoph |
This contribution was helpful to1 thankful Users |
Follow us on