10/13/2018 10:38 AM | |
Posts: 3 Rating: (0) |
hi i have a redundant PLC system with two 412-5H CPU and i want to build and SCADA system on two redundant PC for monitor and control the processes. i have two questions about this: 1) can i use CPU PN port for this means and achieve complete redundancy OR i need cp443 for that? do i need CP1623 for OS or i can use normal network adapter instead? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/16/2018 11:49:19 AMNew subject after splitting. Division of questions into seperate topics. |
|
Follow us on