12/11/2018 8:49 AM | |
Joined: 9/28/2018 Last visit: 10/13/2023 Posts: 7 Rating: (0) |
Hello, I have a same problem. I create a connection between PLC and PC and everything is fine. When I disconnect the PC and connect PLC to the printer nothing send to the printer. In fact I want to connect the PLC to domino printer using CPU 1500. Can Someone help me? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/11/2018 10:41:41 AMNew subject after splitting |
|
12/11/2018 11:32 AM | |
Joined: 7/9/2015 Last visit: 4/24/2024 Posts: 3812 Rating: (554)
|
Hi, do you use intern PN interface of PLC 1500? Then you use the T-Blocks. These blocks have output parameters like Error / Status - please check/save Status when Error gets true. If you use S7-1500 you don´t need to use TCON - please check this: How you configure a connection in the TIA Portal?Regards, Towome |
|
|
This contribution was helpful to1 thankful Users |
7/2/2019 9:59 AM | |
Posts: 3093 Rating: (322)
|
Hello, How do you evaluate the status of system blocks in STEP 7 (TIA Portal)? Does the printer use an unspecified connection? Regards, |
8/27/2019 1:11 PM | |
Posts: 2 Rating: (0) |
Hi, we have a tool, to easily connect OPC UA to Domino. So you could bridge the OPC UA Server from the S7-1500 to your printer. See a screenshot here: OPC UA <-> Domino br inray
|
Follow us on