12/20/2018 7:39 PM | |
Joined: 3/9/2012 Last visit: 8/10/2024 Posts: 236 Rating: (0) |
Hello i am Teo, i have 4 Inverter G120C but in Tia Portal i can set 4.7.9 Firmware. My Inverter are 4.7.10 and i have error. i want to install SINAMICS_G120_firmware_V4_7_HF11.zip (79,0 MB) how can i do that ??? Thanks |
12/20/2018 9:28 PM | |
Joined: 3/9/2012 Last visit: 8/10/2024 Posts: 236 Rating: (0) |
Hello Hati, Where I can download all updates to be sure I am ok. Because I cannot find 4.7.10 |
12/21/2018 6:26 AM | |
Joined: 5/12/2006 Last visit: 9/24/2024 Posts: 22371 Rating: (3014)
|
Hello, in the zip file is the FW for the G120 no data for install in Startdrive(TIA). The HSP V4.7 SP10 can be downloaded here https://support.industry.siemens.com/cs/ww/en/view/109754382 in TIA go to Options -> Suport Packages , navigate to the folder with the extracted HSP Data and install it. I'm not sure if TIA Updater load the Startdrive HSP .
|
This contribution was helpful to1 thankful Users |
12/21/2018 6:35 PM | |
Joined: 3/9/2012 Last visit: 8/10/2024 Posts: 236 Rating: (0) |
Hello, i have download all updates and Startdrive_V15_HSP_FW_V4_7_SP10.zip (460.6 MB) but i cannot set from Tia portal the firmware to 4.7.10.11 this mean 4.7.10 HF1 |
Last edited by: TeoTheNtal at: 12/21/2018 7:03:46 PM |
|
Follow us on