12/29/2018 7:56 PM | |
Joined: 10/6/2018 Last visit: 3/17/2022 Posts: 16 Rating: (1) |
Hi, Is it possible to set the background of the button in another color? I need different buttons and PushButton are green or red. Idem to PlotLights. The button is a simple button with Pushbutton aspect as you explain and lights are PlotLight (L) and a Cyrcle (R): If I link Light to a output, will it work well with a real HMI? With PLCSIM and HMI on Runtime mode is not problem. I checked different videos and people link lights to a mark. Button is a mark. That's ok. Thank you so much Greets ------------------------------------------------------------------------------------------ |
Last edited by: MiguelGT at: 12/29/2018 7:57:06 PMLast edited by: MiguelGT at: 12/29/2018 7:58:31 PMLast edited by: CS Moderator at: 12/30/2018 11:42:43 PMNew subject after splitting |
|
12/31/2018 8:25 AM | |
Joined: 4/24/2006 Last visit: 9/26/2024 Posts: 8742 Rating: (1168) |
Hello, When you use Simulation, does it function like you want? Best regards, Wizard |
Follow us on