12/30/2018 2:03 PM | |
Joined: 12/3/2018 Last visit: 1/22/2024 Posts: 76 Rating: (0) |
I don't understand the purpose either ;) So let's go back to more specific and less philosophic things: I would like to use Cursor arrow to change the Automatic/Manual mode. The idea is to keep the button pressed for 3 seconds not to switch unintentionally. If I do it in LogoSoft simulator or directly on Logo itself, it works OK. I would like to do it via Web server or Siemens Logo application as well, but the problem is, that Cursor button works only as momentary switch. I assigned it as "Switch" in simulation properties, but it doesn’t help me… In WEB server it goes up and down immediately, regardless of how long I keep it pressed. So, how can I do it in the way I planned? [snip] ... ---------- second question split to What is the purpose of "Protection active" setting? ------------------------------------------------------------------------------------------ AttachmentAvto_Man_Web server.zip (305 Downloads) |
Last edited by: CS Moderator at: 12/31/2018 2:02:06 PMsplit into seperate threads Last edited by: CS Moderator at: 12/31/2018 2:07:47 PMNew subject after splitting |
|
12/30/2018 5:59 PM | |
Joined: 12/3/2018 Last visit: 1/22/2024 Posts: 76 Rating: (0) |
This solution is just fine as well, I tried with web server and phone app and it works for me. Thank you! [snip] ... ----------- split to LOGO-Display: what is the purpose of blue side and "Lines" in display creating window? and I would like to use several (multiple) screens of Logo display |
Last edited by: Frayer at: 12/30/2018 6:00:47 PMLast edited by: CS Moderator at: 12/31/2018 2:28:46 PMseperated follow up questions |
|
1/3/2019 12:53 PM | |
Joined: 12/3/2018 Last visit: 1/22/2024 Posts: 76 Rating: (0) |
I found further explanation of behavior for Cursor keys in Web server here: https://support.industry.siemens.com/cs/mdm/100761780?c=64613005067&lc=en-WW
|
Last edited by: Frayer at: 1/3/2019 12:56:08 PM |
|
This contribution was helpful to1 thankful Users |
1/3/2019 7:35 PM | |
Joined: 12/18/2014 Last visit: 10/10/2024 Posts: 33927 Rating: (4217)
|
Have you test it? It doesn't work continuous, only as a pulse input |
Follow us on