2/12/2019 3:51 AM | |
Joined: 9/9/2015 Last visit: 9/25/2024 Posts: 727 Rating: (278) |
Dear All, I would like to share a tip related to IS server. I'm using PH and IS in a separate station - version 2014 SP3 Update 1. PH is running good but IS is not working. The error showing in IS is : "Report generation failed: An error has occurred during report processing. An SQL occurred: A .NET Framework error occurred during execution of user-defined routine or aggregate "udf_GetTagValueAggregateSeriesPrecise". After troubleshooting, I found Trial licenses activated. After deleted the trial licenses, it works without issue. Issue resolved. AttachmentSQL Error.zip (229 Downloads) |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
This contribution was helpful to2 thankful Users |
Follow us on