3/27/2019 4:32 PM | |
Joined: 6/29/2018 Last visit: 4/24/2024 Posts: 17 Rating: (0) |
Hello , I am using DCC charts and I want to read a parameter from servo unit ( it is the speed in rpm ) in order to use it for my further calculations.I can create new parameters successfully and they are displayed on the expert list.The problem is that when I go into the test mode, the read value is not correct. For example instead of reading a speed = 40 rpm ,the shown value is 0.002 .Is there any particular block used to read parameters ? Thank you ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 3/28/2019 12:59:54 PMNew subject after splitting |
|
3/28/2019 11:39 AM | |
Joined: 6/29/2018 Last visit: 4/24/2024 Posts: 17 Rating: (0) |
Hello , Thank you . Now it is working . |
Follow us on