(4)| 5/20/2019 9:44 AM | |
|
Posts: 5521 Rating:
|
hi, S7-1200 CPUs are supporting simulation from FW-version 4 and higher. Use a project with a CPU with higher FW and try to simulate again. regards, |
| 5/20/2019 10:16 AM | |
|
Posts: 2826 Rating:
|
Ensure not to mix the versions V15(.0) and V15.1. Use the PLCSIM version that is compatible with the Step7 version you have installed. Perhaps make a screen-capture and share it here of which softwares you have - if you want someone to check. Please source the installation from: (assuming TIA V15.0) |
| 5/20/2019 10:28 AM | |
|
Posts: 58 Rating:
|
yes, I have downloaded PLCSIM V15.1. Because i didnt get V15.0. And the link which you provide have 3 Setup,out of which one is right Please help me. |
Follow us on