5/28/2019 8:47 AM | |
Joined: 4/24/2006 Last visit: 8/30/2024 Posts: 8728 Rating: (1166) |
Hello, Perhaps it happens, because there was three times an incorrect password, see the following link: Why can you no longer log on to the operator panel (or WinCC flexible Runtime)? When you change "the number of invalid login attempts" to 'zero' it will be solved. Best regards, Wizard |
This contribution was helpful to1 thankful Users |
5/29/2019 5:27 PM | |
Joined: 9/21/2012 Last visit: 9/1/2024 Posts: 4126 Rating: (462) |
I'm with Wizard on this, this is the most common reason.The display doesn't "forget" the passwords, the system just locks the user if too many incorrect passwords have been entered. |
This contribution was helpful to1 thankful Users |
Follow us on