5/28/2019 12:27 PM | |
Joined: 8/1/2012 Last visit: 7/16/2024 Posts: 76 Rating: (3) |
[snip] A bit of out topic, but, is there a proper way to activate the runtime for the OS? Can this be activated from the ES or just manually activate from the OS itself? Regards, wantutri ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/29/2019 09:23:17New subject after splitting. Division of questions into seperate topics. |
|
5/28/2019 12:32 PM | |
Joined: 3/14/2008 Last visit: 8/10/2024 Posts: 2082 Rating: (931)
|
Hi, Good it solved your problem! Runtime should be activated on the OS server itself (autostart is possible, so WinCC runtime will start automatically after you reboot the PC of the OS server). You should not run OS runtime on your ES station as this can cause problems (especially with user archives). You can however use ES simulation. You activate a simulation of the project on your ES station. For this, you need to create a netpro connection between ES-OS station. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
5/28/2019 2:51 PM | |
Joined: 8/1/2012 Last visit: 7/16/2024 Posts: 76 Rating: (3) |
Thanksss |
5/29/2019 10:49 AM | |
Joined: 5/3/2017 Last visit: 5/21/2024 Posts: 673 Rating: (217) |
Hello wantutri, an additional information. If you activate the OS runtime on the ES (excluded OS Simulation) this will cause problems. In this case you have to follow the FAQ What should you do if the OS server project is taken online by mistake on the ES?. With regards |
Follow us on