7/12/2019 5:26 PM | |
Posts: 14 Rating: (0) |
Hello. I programming light control with WEB button and physical buttons. Need to make web light control and physical buttions control have a question how to make that? attached one button scheme. The problem is that here work only physical or only web buttons. How to do web and physical control together? Why with NQ1 block non't work web control. AttachmentDesktop.zip (157 Downloads) |
Last edited by: fenixas969 at: 07/12/2019 17:48:57 |
|
7/12/2019 5:29 PM | |
Joined: 12/18/2014 Last visit: 9/21/2024 Posts: 33810 Rating: (4201)
|
And what should that tell us? |
7/12/2019 6:15 PM | |
Posts: 14 Rating: (0) |
Thanks for so fast answer. Yes I need an example, please attached |
7/12/2019 6:42 PM | |
Joined: 12/18/2014 Last visit: 9/21/2024 Posts: 33810 Rating: (4201)
|
In the attachment is the example. In order to generate a dynamic signal from a static signal from the web server, a network output with the same address must always be held at 0 signal by LOW block. Attachmentfenixas969.zip (177 Downloads) |
7/12/2019 7:19 PM | |
Posts: 14 Rating: (0) |
Thanks. Yes it works, but I need to work from one web button and not from two. How to do it? |
7/12/2019 7:23 PM | |
Joined: 12/18/2014 Last visit: 9/21/2024 Posts: 33810 Rating: (4201)
|
There's only one web button. The other digital value is only for showing the state of Q1. |
7/12/2019 7:27 PM | |
Posts: 14 Rating: (0) |
It is possible to do on one button web button and digital value for showing the state? |
7/12/2019 7:28 PM | |
Joined: 12/18/2014 Last visit: 9/21/2024 Posts: 33810 Rating: (4201)
|
No. |
7/12/2019 7:32 PM | |
Posts: 14 Rating: (0) |
That's too bad But still thanks for your help |
Follow us on