8/20/2019 11:01 AM | |
Joined: 5/29/2013 Last visit: 5/2/2024 Posts: 100 Rating: (28) |
Win 7 Ultimate - V15.1 update 2 (Safety advanced/opennnes/Wincc professional/Startdrive). On Host and VMware. Probably everyone would like to see some changes to Tia portal, but I don’t have the feeling that everyone really mention them to Siemens. I tried to do that in the past, and then I also understand why they don’t be mentioned anymore. Despite that I wanted to just give it another try. So I made a list of 34 general points in the hope that someone at Siemens (higher ranked than the automation support development note list) also read this and really does something with it. This list is limited to daily used functions so I’m not getting really into de wincc advanced and professional, properties of hardware etc. At the end we all want a better TIA Portal. So let’s make V16 changing the world. Below its just the index of the PDF document that I have attached: FBD 1.Disable automatic jump on enter.4 2. Jump labels in empty networks.4 3. Multiple SUB inputs on the SUB instruction.4 4. Tmail_C send LOG/CSV file instead of the BIN file as attachment.4 Compiler 5.Acknowledge warnings.5 General 6. Bigger minimize maximize and close button in the upper right corner.5 7.Auto save.5 8.Find&Replace with incremental counter.6 9.Replace all is not working on tag tables.6 10. Let TIA use all the power I have in my notebook.6 11.Remove the T# input also in the data blocks time values.6 12. Online toggle Boolean by double clicking annoying popup.6 13. Auto fill decimal place by offline real value in datablock.6 14.Save archive on same location as Project folder.7 15. Tia portal updater.7 16.Safety i/o state during commission i/o check.7 17. Monitoring values in datablock.7 18.Whats new in this version ?.7 New Instructions 19.GetProjectName.7 20.String to SymbolName.8 21.New feature to do indirect addressing in optimized db’s.8 22.Reset_Array / Reset_Struct.8 Analizing 23.CycleTime analyser.8 Hardware 24.TM_Count 1x24V..8 25. T models for ET200SP CPU’s and 1505/7/8 software controllers.9 HMI 26. Appearance Tag suggestion from the event.9 27. Boolean should be an button instead of i/o field.9 28. Default disable focus.10 29. KTP 300 smallest font size depending on windows settings.10 30. Shortcut also to HMI tag, like the green arrow for PLC tag.10 31. COPY paste alarms doesn’t copy the triggertag.10 32.Remember screen zoom settings. And open all following screens in the same zoom..10 33. Representation setting for time values.10 34. That never ending AM/PM or 24 clock setting10 AttachmentTia Portal recommendation for V16.pdf (2123 Downloads) |
Last edited by: Ikkez at: 08/20/2019 11:06:22Regards |
|
This contribution was helpful to16 thankful Users |
Follow us on