10/20/2019 6:02 PM | |
Joined: 4/3/2019 Last visit: 2/20/2024 Posts: 116 Rating: (1) |
maybe there are some libraries for such a functions? something easier and quicker ? |
10/20/2019 6:27 PM | |
Joined: 12/18/2014 Last visit: 9/19/2024 Posts: 33794 Rating: (4199) |
Take a look at this library: Library of general functions (LGF) for SIMATIC STEP 7 (TIA Portal) and SIMATIC S7-1200 / S7-1500 In this library is a function for a weekly timer. |
10/20/2019 7:29 PM | |
Joined: 4/3/2019 Last visit: 2/20/2024 Posts: 116 Rating: (1) |
I have TIA portal v15 and this is for 15.1 when I try to load this library I get error... |
10/20/2019 7:33 PM | |
Joined: 12/18/2014 Last visit: 9/19/2024 Posts: 33794 Rating: (4199) |
Then download the V14 SP1. Then you can open it and upgrade it with V15. |
Follow us on