1/11/2020 2:52 AM | |
Joined: 3/8/2019 Last visit: 7/26/2023 Posts: 14 Rating: (0) |
Hi Georg Berghof, I'm not sure if these are internal tags because I review all the tags in Tags Management but I cannot see the uncreated tags that assign in IO filed. There's a lot of tag also that uncreated but it's still work without a problem. Their's one thing I found last day while migrating my project that I have 5 C scripts were not successfully migrated. Maybe this is also the problem. I attach photos of the diagnostic message that pop up while migrating the project. Please kindly see below. Thank you very much Sir Georg Berghof for trying to help me. Regards, Honey AttachmentDiagnostic Msg.zip (90 Downloads) |
Follow us on