1/15/2020 6:13 PM | |
Posts: 1 Rating: (0) |
Hello members, I am trying to connect tia portal to nx mcd, I have technology object (positioning axes). can I connect the technology object directly from tia portal to MCD without simit? ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 01/15/2020 19:23:21New subject after splitting |
|
1/16/2020 4:58 PM | |
Joined: 12/10/2018 Last visit: 11/28/2023 Posts: 1 Rating: (0) |
You are able to connect an technology object to an MCD signal without SIMIT. If you are using a physical PLC you can access the data by OPC UA. Reccomended is to use PLCSIM Advanced and access the data by the PLCSIM Advanced API of MCD. If you want to move an object simply connect the signal to the actual position of the technology object. Please check the information and example project below how this is done. [permanent link to parent page: https://support.industry.siemens.com/cs/ww/en/view/109760078 ] Best regards, Jelle |
Last edited by: AutoGen_6425089 at: 01/16/2020 16:59:01Last edited by: The Helping Hand at: 01/16/2020 17:18:49Added permanent Link |
|
Follow us on