2/17/2020 7:28 AM | |
Posts: 2 Rating: (0) |
Hello All! I have a controller S7-1200 (CPU1214C DC/DC/DC) with module SM1231 (6ES7 231-4HD32-0XB0). Module Documentation 13-bit. i am using 5 ton loadcell.how can i calculate. ------------------------------------------------------------------------------------------ |
Last edited by: ramu1985 at: 02/17/2020 09:28:55Last edited by: Jen_Moderator at: 02/17/2020 14:16:04New subject after splitting |
|
2/18/2020 6:30 PM | |
Joined: 4/18/2019 Last visit: 10/1/2024 Posts: 33 Rating: (0) |
Hi not sure if the link works, but I used a sm1231 in 4-20 ma mode, this was reading a 0 to 60 bar pressure gauge. this shows how i did it as I asked for advice for vacuum gauges it was in the step 7 tia portal page hope this helps Analog input advice, I need help using vacuum gauge with 0-10 volt output |
Follow us on