7/4/2020 7:04 AM | |
Joined: 5/13/2019 Last visit: 2/8/2021 Posts: 10 Rating: (0) |
Thanks Scorp for the suggestion. I just now got around to check it. Also I have a free day today to play with the tanks. When I check with simulation I see that the displayed ma to logo screen when I move the analog bar from 0 to 1000 goes to 250,5ma but should be only 20 ma displayed as sensor 1. Can someone please check the scale for sensor 2 that is correct. and change the display for me to be in a range 4-20ma with 2 decimals as it is on sensor 1? Or someone give me directions of which block number I need to modify. I wan to do this and install program and then as scorp suggest me to measure the volume of the tank. I wan to do this by water (e=1kg/L) but in parallel I wan to take the readings of ma from the sensor on logo screen. Thanks in advance Chris ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 07/06/2020 06:02:43New subject after splitting |
|
7/6/2020 6:04 AM | |
Joined: 6/19/2017 Last visit: 5/13/2024 Posts: 8033 Rating: (163) |
Closed cause question posted twice. The second thread with the subject Scale 4-20mA sensors is published within the conference LOGO! - Projects. Best regards,Jen_Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on