10/7/2020 7:15 PM | |
Joined: 9/27/2006 Last visit: 5/5/2024 Posts: 12257 Rating: (2666) |
Hello; The only documentation on Lika RD4 Profibus configuration with a S7 CPU is based on Step 7 v5.x: http://www.controldevices.com.au/product/rd4-series-heavy-duty-rotary-actuator/ It explains how to configure, parameterize and program the RD4 rotary actuator as a Profibus slave to a Profibus master in Step 7 v5.x. You can follow the information from the TIA Portal v15.1 system manual to do the same with, for example, a S7-1200 with a CM 1243-5 Profibus master. Other families of CPUs are available in the manual if needed. https://support.industry.siemens.com/cs/ww/en/view/109755202/116759554059 Hope this helps, |
Last edited by: dchartier at: 10/07/2020 19:15:36Last edited by: dchartier at: 10/07/2020 19:43:11 |
|
Follow us on