12/11/2020 5:55 PM | |
Posts: 18 Rating:
|
Hello, I have an IOT2040 running off our machine testing temperatures, weights, etc. from a PLC that I set up a flow using Node-Red. Using THIS tutorial I set up the connection to AWS from the IOT2040 and made sure they could communicate. My next task showing these metrics on a dashboard through AWS. I have a local Node-Red UI page, but we want to be able to pull up the dashboard from anywhere without having to connect to the IOT through ethernet. Curious if anyone has knowledge on what the best route is to take going forward to set up a "webpage" that acts as a dashboard to view all of our machines metrics and data but still through our Node-Red flow. Thanks |
7/11/2022 8:29 PM | |
Joined: 7/11/2022 Last visit: 11/11/2023 Posts: 3 Rating:
|
it worked out? |
7/13/2022 8:52 AM | |
Joined: 4/8/2021 Last visit: 5/14/2024 Posts: 638 Rating:
|
Hi Paul, I'm not a Node-RED expert as I only used if for a couple of times. However I remember that it has some integraded nodes that you could use to create dashbords inside Node-RED. https://flows.nodered.org/node/node-red-dashboard Hope it helps. Br, Cocolino |
Best regards, |
|
Follow us on