3/18/2021 5:58 PM | |
Joined: 7/12/2018 Last visit: 6/13/2024 Posts: 2 Rating: (0) |
I have a very similar situation. Newly compiled example image on SD Card with BalenaEtcher Solid Green Stat/Power LED after 10 minutes. No Communication on default 192.168.200.1 P1 Ethernet No Video In addition, I am not getting any messages from USB UART. I have two units and the other one works fine, I can see messages on the putty console. Any other recommendations? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 03/19/2021 09:34:26New subject after splitting. Removed image, which was embedded in the text and added it as a file. |
|
This contribution was helpful to1 thankful Users |
Follow us on