4/26/2021 10:57 AM | |
Joined: 2/27/2020 Last visit: 5/9/2024 Posts: 9 Rating:
|
Hello guys, I am facing some issues communicating with MiR robot using LHTTP. I have adjusted the LHTTP_Get function to include required headers (authorization, accept-language), but I get error 8408 all the time (Request timeout. Check the Ethernet connection of the PLC and the URL.). URL with headers was previously tested with Insomnia client and exactly the same URL is working perfectly fine. I am using Scalance S615 router with open port 80 and I can ping the robot's IP from there. Also tried connecting PLC directly to network with no success. Anyone encountered similiar issues? Or has any ideas? - - - EDIT: Found out Company network was the issue, firewall was blocking the connection on port 80 and for IT security reasons I am forced to use HTTPS. Unfortunately I haven't got through SSL verification yet... getting error 80E4. Not sure how to force client to trust server since setting tls.validateServerIdentity to FALSE does not seem to be enough. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 04/26/2021 13:01:34New subject after splitting Last edited by: MartinGio at: 04/30/2021 13:16:10 |
|
5/27/2021 10:16 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating:
|
hi, did you have a look into the documentation, chapter 2.4 Error handling? look what I found: 400 Bad Request The request message was structured incorrectly. hope this helps, regards, |
FCK WAR! |
|
12/20/2023 10:56 PM | |
Joined: 12/19/2023 Last visit: 12/20/2023 Posts: 1 Rating:
|
HELLO MARTIN CAN YO SHARE WITH ME THE PROGRAMME THAT YOU ARE USED TO COMMUNICATE WITH MIR ROBOT THANKS |
Follow us on