10/4/2021 4:18 PM | |
Joined: 12/18/2014 Last visit: 5/10/2024 Posts: 33002 Rating: (4078) |
HF1 for S7 Technology V4.2 SP5The HF1 for the operation of S7 Technology V4.2 SP5 under STEP 7 V5.7 is available. This hotfix is required to use S7 Technology V4.2 SP5 in combination with STEP 7 V5.7. For older versions of STEP 7, the HF1 is not required. S7 Technology V4.2 SP5 HF1 does not include any functional changes compared to S7 Technology V4.2 SP5. HF1 is free of charge and only available as download version under the entry ID > 109799562 First install S7 Technology V4.2 SP5 and then the HF1. Installation requirements The following operating systems are supported:
|
Last edited by: ixo65 at: 10/04/2021 16:19:25 |
|
Follow us on