3/5/2009 9:28 AM | |
Joined: 4/24/2006 Last visit: 9/20/2024 Posts: 8742 Rating: (1168) |
Dear sharo, The option can you buy at Danfossrepresentative. Here is a link to manual: http://www.danfoss.com/BusinessAreas/DrivesSolutions/Documentations/Technical+Documentation.htm select VLT automation drive FC300 Then under options you select 'Converter (2)' Right now it is possible to download manual "VLT 5000 Profibus to FC 302 converter" Hope it might help you. Best regards, Wizard |
3/5/2009 10:05 AM | |
Posts: 12 Rating: (0) |
I search on internet and I found that the MCA 114 option that you talked to me, it's a conversion kit. then it must be purchased?? |
3/5/2009 11:17 AM | |
Joined: 4/24/2006 Last visit: 9/20/2024 Posts: 8742 Rating: (1168) |
Hi, |
3/5/2009 12:10 PM | |
Posts: 12 Rating: (0) |
I changed the hardware configuration and the address assigned to FC300.
Now, I must change the program. So, I have to add new instructions or I have just to change the address of the variable depending on the type used in FC300? |
3/6/2009 9:24 AM | |
Joined: 4/24/2006 Last visit: 9/20/2024 Posts: 8742 Rating: (1168) |
Dear sharo, Depends on the used PPO type when using VLT5000 and the PPO type you want to use now. When it is PPO type 3, it is just the right addresses and it should work. Best regards, Wizard |
3/6/2009 10:59 AM | |
Posts: 12 Rating: (0) |
Hi Wizard, This means that I must use in FC300 the same PPO type used in VLT 5000? you said, When it is PPO type 3, it is just the right addresses and it should work. Pleaaase, explains me what this means What about the other type of PPO?It could not work by just changing addresses? |
Follow us on