1/19/2022 1:43 PM | |
Joined: 8/3/2009 Last visit: 5/3/2024 Posts: 12882 Rating: (1643) |
Hello Nejedly10 you can only use the controls that are available in Report Designer, Alarm Control and Trend- or Tablecontrol. Here you can use Filter Strings for time period. (Here a little example für the string building, its a quite old FAQ but still works) To print the protocol you can use a C Script standard function for this. -> If you want a more user specific export then you could use PM OPEN Export or Information Server for example to work with SQL Reporting Services Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on