5/6/2016 9:10 PM | |
Posts: 163 Rating: (2) |
Picture 6 |
Last edited by: Idir at: 5/6/2016 9:14:13 PM |
|
5/6/2016 9:24 PM | |
Posts: 163 Rating: (2) |
Picture 7, Please guys. Any idea?. it has been a while since i have it now. Regards, |
Last edited by: Idir at: 5/9/2016 8:55:18 AM |
|
5/11/2016 8:47 AM | |
Posts: 163 Rating: (2) |
Diagnostics buffer of the module Master [CPU 315-2 DP] AttachmentDiagnostic Buffer.txt (45 Downloads) |
Last edited by: Min_Moderator at: 5/11/2016 1:50:30 PMAdd attachment |
|
5/11/2016 9:06 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1050) |
hi Idir, I´m a little bit confused now, because now you are working with TIA. Your CPU is only supported by TIA since FW-Version V2.6. But yours have V2.0 What FW-version do you have projected and loaded on it? With Step7 5.5 or TIA? Maybe the parameter assingment-error occurs because of wrong FW or a FW-Bug. Here you can find the download of actual FW and instructions to update it: Operating System Updates for CPU 315-2DP hope this helps, regards, |
FCK WAR! |
|
5/11/2016 9:19 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1050) |
hi Idir, please read carefull what I write. then answer to the questions I asked. regards, |
FCK WAR! |
|
5/11/2016 9:47 AM | |
Posts: 163 Rating: (2) |
Why is there no way? |
5/11/2016 10:04 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1050) |
see this FAQ: Which devices and modules are supported by STEP 7 Professional and WinCC Professional in the TIA Portal?As you can see in the table the 6ES7-2AG10-0AB0 is compatible with TIA from FW-version 2.6 The devices must be projected with the rigth FW-Version. Some CPU´s can be projected with older FW-versions, they are downwards-compatible, but never with newer version. With a new FW you have new features on CPU, so when you project a 2.6, with features that the 2.0 doesn´t know, there will be errors like the parameter assignment error. hope this helps, regards, |
Last edited by: mopS04 at: 5/11/2016 10:05:21 AMFCK WAR! |
|
Follow us on