Industry Online Support
Technical Forum
7/8/2010 8:18 AM | |
Joined: 2/24/2009 Last visit: 3/4/2024 Posts: 26 Rating: (0) |
Nobody knows or nobody cares? |
7/8/2010 9:12 AM | |
Joined: 4/24/2006 Last visit: 4/19/2024 Posts: 8610 Rating: (1147)
|
Dear andrej5, Perhaps the following links might help you: Which settings are required in Windows 2000, Windows XP, Windows Vista and WinCC flexible for server-client communication via OPC XML? Which settings are required in Windows XP SP2 and WinCC flexible for server-client communication via OPC-DCOM? Best regards, Wizard |
Follow us on