1/19/2021 6:35 PM | |
Joined: 1/12/2021 Last visit: 9/9/2023 Posts: 1 Rating: (0) |
I have been using the OB121 with the PLCSIM ,The CPU 315-2DP Now with the TEMP variables using the OB121_PRG_ADDR Doesn't seem to give the exact relative address 1 .is there a way to get the exact fault address 2.SF Fault LED seems to be cleared only after switching between the stop mode and then back to the run mode,is there a way this can be done without switching between the two operation modes? Thanks ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 01/20/2021 08:40:35New subject after splitting |
|
Follow us on