6/22/2009 10:24 AM | |
Joined: 10/7/2005 Last visit: 4/26/2024 Posts: 3004 Rating: (1046) |
Dear darkvader looks like the "force" was not with you on this one and I have a bad feeling that you "lost" your S5 program due to a missing or empty backup battery. If this is the case, you will need to find a backup and download it again to your CPU. Have a look at this link where you will find the 115U manual which explains all the ISTACK entries (see Chapter 5: Error diagnostics) and everyting else you need to know aboutdealing with this type of S5. I hope this helps even though I have a feeling that I am the bearer of bad news for you. Cheers Fritz |
Last edited by: fritz at: 6/22/2009 10:28 AMI guess mumbles beat me to the answer... Cheers |
|
This contribution was helpful to1 thankful Users |
12/21/2015 10:34 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4774 Rating: (123) |
New question published by Super123 is split to a separate thread with the subject PLCS5-115U, Errors. Best regards |
Follow us on