8/28/2009 5:29 PM | |
Posts: 95 Rating: (0) |
Disney I had the same situation as you describe. I was able to get Siemens Tech support to help design the precharge circuits. The Sitor fuses, timing relays, and resistors are all available. All you need is assistance picking the values of the resisters. You can refer to the literature of the cabinet units Siemens builds and see the drawings for more information. In my system, I use a simple selector switch to control the DC bus connection to the motor module. In the off position, the motor module is disconnected from the DC buss. When the selector switch is turned on, a timing relay simply diverts the DC bus through the resistors and then after the preset time, connects the DC bus directly to the motor module. It can be done. Attached is a sheet showing some component part numbers. AttachmentSINAMICS S120 Pre-charge components.pdf (1242 Downloads) |
7/31/2013 9:43 PM | |
Joined: 4/24/2009 Last visit: 8/20/2024 Posts: 2682 Rating: (135) |
New question was splitted to6SE7031-8EF60Z , 125Hp drive with a burned precharge resistor Best regards O_Moderator
|
6/14/2016 1:55 PM | |
Joined: 8/21/2014 Last visit: 9/19/2024 Posts: 1024 Rating: (14) |
New question published by AutoGen_1011712 is split to a separate thread with the subject Precharge circuit Sinamics S120. Best regards |
My Forum is the place to personalize your profile, |
|
8/31/2017 12:56 PM | |
Joined: 8/21/2014 Last visit: 9/19/2024 Posts: 1024 Rating: (14) |
New question published by AutoGen_119085 is split to a separate thread with the subject I need to know how much is power for 6SX7010-0AC10 (resistor 10ohm )?. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on