10/15/2009 1:45 PM | |
Joined: 7/8/2009 Last visit: 7/26/2023 Posts: 1974 Rating: (477) |
Thanks My ID: vithanidevesh@gmail.com Thank you again and Happy Diwali,
|
Last edited by: O_Moderator at: 10/15/2009 2:11 PMnew subject after splitting I dont Like people driving Fast, thats the reason I overtake them ;) |
|
10/16/2009 11:58 AM | |
Posts: 739 Rating: (55)
|
Level 4 parameters are only for development and system test, please don’t use it! |
1/17/2015 12:04 AM | |
Joined: 1/17/2006 Last visit: 5/1/2024 Posts: 552 Rating: (29) |
Hi. I have a converter from manufacturer WEG model CFW11 and there are some parameters (p0156, p0157 and p0158) to define three levels for Motor overload current at 5%, 50% and 100% of its rated speed so an alarm is generated and the motor stopped. Calm down, I don't want info about this brand. My doubt if its possible to do something like this with MM440 without using free/bico blocks? With this drive from Weg when the rotor is blocked an alarm is shown and the drive is disabled for overload. Motor overtemperature based in i2t generates another type of alarm. please see the graphic attached for best undestanding. best regards. Attachmentoverload_CFW11.pdf (255 Downloads) |
"Educate the children and it won't be necessary to punish the men." |
|
2/16/2018 10:58 AM | |
Joined: 6/19/2017 Last visit: 5/13/2024 Posts: 8033 Rating: (163) |
New question published by safaa2 is split to a separate thread with the subject Need to know the value of some parameters of level 4. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on