10/19/2009 9:07 AM | |
Joined: 5/28/2008 Last visit: 6/29/2024 Posts: 4510 Rating:
|
Dear Tomy Master, I am afraid that Aret solution may not working. He was tring to minimize the cost for you, Tommy. I am not sure that CPU314IFM has a DP port or not. But if I remeber well, I think it has not. And becuse if we will insert a CP for MPI communication, we have to add it in HW config and download the modified HW config on the CPU. But if the MPI port has been damaged, so, you can not modify the program. as you won't be able to download the new program on the CPU. And for this CPU (314-IFM) "Internal Flash Memory" it means that there's no flash memory can be inserted into the CPU, so you can not use PG or promer for this purpose. The important question now, Do you have a backup for the software? If yes, you can then select one of the compact CPUs for replacement. CPU313C will be suitable |
Ayman Elotaify |
|
This contribution was helpful to
1 thankful Users |
8/18/2017 11:25 AM | |
Joined: 6/19/2017 Last visit: 6/28/2024 Posts: 8192 Rating:
|
New question published by damonarso is split to a separate thread with the subject Could not connect the CPU to any PC or HMI. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on