10/22/2009 3:15 PM | |
Joined: 4/5/2006 Last visit: 6/5/2024 Posts: 917 Rating: (63) |
Hi Nil96 , a complete explanation about how PCS7 works on AS RT PO booking license is in Simatic manager help: 1) for PCS7 v7.1 : open an cfc, help, search for book or booked and select "Count and Booking of the PO License" 2) for PCS7 v7.0 (just in my mind so i hope to remebr well) : open project in Simatc Component View up to select chart folder, right click, selsct chharts, move mouse on "BookBack Process Object" without click mouse, press F1 for help Hope can help Regards |
10/22/2009 10:07 PM | |
Posts: 2661 Rating: (279)
|
Hi Nil96, The topic of AS RT PO is a touchy subject and has been nicely discussed before in the following thread: PCS7 Licence more understanding |
10/23/2009 9:40 AM | |
Joined: 4/5/2006 Last visit: 6/5/2024 Posts: 917 Rating: (63) |
Hi Nil96 , How bookback license and how to rescue license after CPU failure is described in Simatic Manager help as well as i said above : you have to broken CPU and memory card both to loose PO, if you broke CPUor memory card ONLYsimatic Manager is able to know how many PO has to be resued when you open same PCS7 project. (More detailed info for all scenario in S7 help) (In attach copy of S7 help for lazy people ) About different PO in winCC and Simaic Manager have a look above to your previus post, i answered to this question too Process Object count with a user define FB in a PCS7 Project Regards AttachmentBookBack License.zip (371 Downloads) |
10/23/2009 10:40 AM | |
Posts: 15 Rating: (0) |
a good FAQ: http://support.automation.siemens.com/RU/view/en/38855207 |
This contribution was helpful to3 thankful Users |
9/28/2015 4:46 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4770 Rating: (123) |
New question published by saravana@profi is split to a separate thread with the subject PCS7 V8.2, Error while compilingthe OS "RPC server is unavailable". Best regards |
Follow us on