11/4/2009 7:43 PM | |
Joined: 5/28/2008 Last visit: 4/15/2024 Posts: 4505 Rating: (835) |
Dear Kthalji, For this case put the following parameters: P0700[1] = 2 P0701[1] = 1 "Function of DIN1: "On /Off" for remote start and stop" P1000[1] = 1
You can make P1080[1] = 40 "Minimum Frequency" Also have a look on the attached picture which descripe the timing diagram for both setpoint frqueny and P1080 and actual output frequency. Hope this helps. |
Ayman Elotaify |
|
11/5/2009 4:40 AM | |
Joined: 8/21/2008 Last visit: 3/18/2024 Posts: 141 Rating: (6) |
hi kthalji, I 100% agree with ayman. Please go through the attached document for more details. hope it will be useful to u. rgds, RBM
AttachmentDrive_command_data_sets.pdf (360 Downloads) |
Last edited by: RBM at: 11/5/2009 4:40 AM |
|
11/10/2009 4:50 PM | |
Joined: 11/5/2008 Last visit: 7/20/2011 Posts: 64 Rating: (1) |
Very good information about the CDS change. |
Follow us on