5/8/2019 1:47 PM | |
Joined: 9/19/2011 Last visit: 4/24/2024 Posts: 138 Rating: (33) |
You are using the wrong connection diagram for a two wire 4-20mA transmitter. You should be using the diagram in the attachment. You do not need an external resistor if you configure the inputs as current inputs. Also you can select the 4-20mA range instead of the 0-20mA range. This may make your scaling easier. I recommend that you study the S7-1200 System Manual especially chapters 4, 5, 6, and 7. It is available here: https://support.industry.siemens.com/cs/us/en/view/109764129 |
Last edited by: Jen_Moderator at: 05/09/2019 08:25:21Optimized link. |
|
Follow us on