11/7/2014 5:47 AM | |
Joined: 1/28/2009 Last visit: 5/2/2024 Posts: 6838 Rating: (1359)
|
Hello, When the PLC project is developed in STEP 7 V5.X and you want to use the tags and symbols in TIA environment , I suggest watching a video and reading more about "Device Proxy" in the following link: Combined configuration with WinCC (TIA Portal) and STEP 7 V5.x
I hope this helps, Hamid Hosseini |
This contribution was helpful to1 thankful Users |
11/8/2014 2:09 PM | |
Joined: 1/28/2009 Last visit: 5/2/2024 Posts: 6838 Rating: (1359)
|
Hello again, I think this procedure is not intended for H-CPUs like "6ES7 417-4HT14-0AB0".There is a possibilty to create a new S7-400 (Not an S7-400H) station and copy one of the H racks from HW Config(without sync modules) to new project and compile the new station.In this manner, all blocks and symbols from old project is transferred to new one.Try it this way but note that the new project doesn't retain all H capabilities plus connections from netpro, so it can not be downloaded to CPU.
This is an end to support I can provide here,Please ask "Support Request" for more advice for HMI side. |
Follow us on