(0)| 6/16/2010 12:39 PM | |
|
Posts: 8 Rating:
|
Dear Expert In the SM321- maximum cable length, shielded is 1000m & maximum cable legth, unshielded length is 600m. Please let me know the size of the cables. |
| 6/21/2010 9:51 AM | |
|
Joined: 5/28/2008 Last visit: 1/14/2026 Posts: 4522 Rating:
|
Hello MBSYSTEMS, There will be no problem with 1mm or even 0.5mm specially there's no high current will follow through the wire I am sure. It looks that that DI is for an Emergency button or a limit switch. So the current that will follow through the cable is equal to few milli Amps. But I recommend to use a separite small power supply for this input and use a relay near the module to energize the input. Back to your last question. There will be no problem with 900 m You can use up to 600 m for un-shield cables & 1000 m for shielded cables. Please check the technical specification of your DI module. You will found it in Module data. |
|
Ayman Elotaify |
|
| 8/3/2015 3:39 PM | |
|
Posts: 4757 Rating:
|
|
Follow us on