Industry Online Support
Technical Forum
11/17/2010 12:45 PM | |
Posts: 69 Rating: (1) |
DEAR SIR, WHILE RUNNING SPINDLE MOTOR WITH EXTERNAL ENCODER, WHEN I COMMAND 1000 RPM, SPINDLE SPEED AT MONITOR FLUCTUATION UPTO 50RPM, IF I TRY TO COMMAND 100 RPM, THAT TIME2 RPM ONLY VARIATION. I CHECKED MOTOR RPM THERE IS NO VARIATION AND FOLLOWING ERROR ALSO INCREASING CONTINOUSLY IN SPINDLE. IF I ENABLE MOTOR ENCODER THERE IS NORPM VARIATION. I CHECKED ENCODE COUPLING AND FOUND NORMAL. NC ARCHIVE FILE ATTACHED HEREWITH. KINDLY HELP ME TO SLOVE THE PROBLEM. ENCODER DETAILS ***************************** MAKE: HEIDENHAIN MODEL : ROD 486 PPR: 2500 INCREMENTAL 1VPP AttachmentNC_17_11_2010.pdf (88 Downloads) |
11/17/2010 1:15 PM | |
Posts: 2964 Rating: (481) |
Hello.... What Control is this? could give us the more details details.... Looks like gear ratios are not entered proper check it out.... Regards, Ekalavya |
Follow us on