2/24/2011 3:23 PM | |
Posts: 2964 Rating: (482)
|
Hi, Check the mechnical load....remove the motor outside and check any errors are present...if motor runs fine then mechnical part need to be checked. If it is vertical motor check the brake is getting released properly. Note: If it is absolute encoder position will get loss.... Error informations are present in this link... https://www.automation.siemens.com/doconweb/content.asp?item=12776&cd=sinumerik_simodrive_04_2010_e&scope=all Regards, Ekalavya |
4/12/2016 7:04 PM | |
Posts: 2 Rating: (0) |
Did you get an answer on this? I am currently experiencing the same problem |
Follow us on