5/27/2011 10:50 PM | |
Joined: 9/27/2006 Last visit: 4/20/2024 Posts: 12256 Rating: (2664) |
Hello Victoria; The recommended installation procedure is to start with Step 7, then install WinCC on your PC. But here is a document that shows how you can manually install the missing components in your project: Instructions If WinCC has been installed before STEP 7 … then you must manually install the AS-OS Engineering and Object Manager components. Procedure as from WinCC V7: Start the WinCC Setup. Select the Runtime Setup in Expert Mode (User-defined Installation > WinCC Expert > WinCC Runtime). For the components to be installed you select AS-OS Engineering and Object Manager. Then it is possible to insert an existing WinCC project into the SIMATIC Manager
http://support.automation.siemens.com/WW/view/en/22272911 Hope this helps, Daniel Chartier |
This contribution was helpful to1 thankful Users |
5/28/2011 8:57 PM | |
Posts: 947 Rating: (45) |
Hello Victoria99 After installing Step 7, you can rerun the installation of WinCC without deinstalation and add missing components, although both said dchartier better first install Step 7 |
Follow us on