9/17/2011 2:33 PM | |
Posts: 54 Rating: (0) |
Dear Sirs, Iam doing a project which has three PLC stations each has redundent PLC.Ihave some questions. I hope you will guide me. 1.Can We UseS7 300(315 2DP)PLC to achieve redundency.If yes then do we needsome specialsoftware or what ? 2.The Control room is located at some distance and we want to connect all three PLC stations to the control room via OPTICAL FIBER;so how we can do that means what hardware we need to add. 3.I have attached the layoutI made For The System.Please Tell Me IfThe Network Has Some Mistakes. Thanks wairing for your reply. Rahil AttachmentFewa_Network_Topology.zip (308 Downloads) |
Last edited by: rahilansari at: 9/17/2011 6:39 PM |
|
9/17/2011 6:35 PM | |
Posts: 54 Rating: (0) |
anyone plz reply |
9/20/2011 9:39 AM | |
Posts: 54 Rating: (0) |
Thanks For Your Valuable Replies. I Used OLM Only Because I Found On Internet AboutOLM,But Iwasn't Sur About That Thats y I Asked. |
9/20/2011 1:14 PM | |
Posts: 8 Rating: (1) |
Hi, This document describes step by step settings to do in step 7... Regards, RDI AttachmentSoftware Redundanz.pdf (337 Downloads) |
This contribution was helpful to1 thankful Users |
2/28/2018 1:35 PM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
New question published by gabbar is split to a separate thread with the subject Can use 6ES7195-7HB00-0XA0 for connecting both whole rack of ET200M, IM153-2 INTERFACE REDUND.BUNDLE.with i/o modules?. Best regards |
Follow us on