(3)| 11/17/2011 4:47 PM | |
|
Joined: 9/27/2006 Last visit: 1/13/2026 Posts: 12480 Rating:
|
Hello Matko; I myself have not done this configuration, so all I can provide you is the S5 to S7 guide for Industrial Ethernet from the Quick Start Simatic Net CD. There are some sample programs and documentation that could guide you. You can find it here: https://www.automation.siemens.com/net-static/Quickstart2009/quickstart012003/html_76/s5-beispiele/beispiele.htm Hope this helps, Daniel Chartier |
This contribution was helpful to
|
|
| 11/19/2011 1:38 PM | |
|
Joined: 10/7/2005 Last visit: 1/12/2026 Posts: 3054 Rating:
|
Hello Matko Good news: You are correct, using a SEND with QTYP = RWmakes it a so called "Active Write" which contains the destination DB/DW numbersand only requires a "Receive All" call in the partner. Not so good news: This may not work any more when anS7 is now the destination (trut he be told, I never tried it). As the destination DB/DW will be part of the telegram, using a "AG_RECV" call may still do the job (an S7 does of course not have a "Receive All" Block anymore) and you would then "simply" ignore the surplus destionation DB/DW header data. Saying that, it may be easier (or even required) to ditch the existing link and configure a new Send/Receive link as well as adjusting the S5 program. Below are a couplemore additional links for this and I hope it helps: Commissioning and Configuring an ISO Transport Connection between the SIMATIC S5 and SIMATIC S7 via Industrial Ethernet Where can you find sample programs and documentation for communication from SIMATIC S5 modules to SIMATIC S7 modules via Industrial Ethernet using the ISO transport protocol? |
|
Cheers |
|
This contribution was helpful to
|
|
| 3/31/2016 2:37 PM | |
|
Joined: 8/21/2014 Last visit: 12/19/2025 Posts: 1098 Rating:
|
New question published by HLetham is split to a separate thread with the subject Replacing S5 by S7-1500. Best regards |
|
My Forum is the place to personalize your profile, |
|
| 1/7/2018 10:52 AM | |
|
Joined: 9/1/2005 Last visit: 1/9/2026 Posts: 4114 Rating:
|
New question published by AdelZein is split to a separate thread with the subject Replace one device with a S7-400 and connect via SINEC H1 network to Wincc. Best regards |
|
My Forum is the place to personalize your profile, |
|
Follow us on