12/14/2011 5:43 PM | |
Posts: 31 Rating:
|
Dear Experts, I m using WinCC 7.0 SP1, and the OS is Windows XP SP3. Everything was great till yesterday. Yesterday i have opened a new project with only 3 simple pdls and a few tags in it no script . Now, the problem i have is; when i m trying to activate project(only winCC explorer is opened) blue triangle is deactivated and blue rectangle is activated(as you can see one of attached image) and i know it is as it should necessary. But no runtime screen at all. On the other hand, if i open graphics designer and try to run pdl it is giving me an error like "Runtime could not be activated! Check the settings in the WinCC control center" Things I have already try: 1- remove .dcf file - (nothing changed) 2- dublicate project (nothing changed) 3- reinstall WinCC 7.0SP! (nothing changed) Please give me a hand. Thanks in advance. Attachmenterror.zip (363 Downloads) |
10/22/2012 7:45 AM | |
Posts: 144 Rating:
|
cool i am in the same situation and i hope this setting will help! |
11/16/2013 5:50 AM | |
Joined: 11/16/2013 Last visit: 7/18/2024 Posts: 28 Rating:
|
Tried mentioned options, RT not activating! Any tips to fixan error? |
Follow us on