1/14/2012 8:07 PM | |
Posts: 5 Rating: (0) |
I am not able to install simatic step 7 basic v11 sp1 on windows 7 64 bit HP dv 6 machine? |
This contribution was helpful to1 thankful Users |
1/18/2012 2:25 PM | |
Posts: 4 Rating: (0) |
Same problem here. So the next question is: When can SP2 be expected? |
1/18/2012 4:31 PM | |
Joined: 4/24/2006 Last visit: 9/26/2024 Posts: 8742 Rating: (1168) |
Hello kweetniet, Sp2 for TIA Portal V11 is released. You can even download it: Servicepack 2 for Step 7 V11 But when you want to install it on Windows 7 64 bits: The download is not suitable for new installations (e.g. on Windows 7 64-bit operating systems). Here you require the STEP 7 Professional V11 SP2 Trial DVD (order no. 6ES7822-1AA01-0YA7). Best regards, Wizard |
1/18/2012 5:45 PM | |
Posts: 5 Rating: (0) |
YES THE DRIVER IS NOT SUTAIBLE FOR NEW INSTALLATION. |
1/31/2012 9:13 AM | |
Joined: 10/10/2005 Last visit: 8/29/2024 Posts: 1917 Rating: (136) |
Hello, there are some FAQs in the internet and could be helpful for you: http://support.automation.siemens.com/WW/view/de/57775228 http://support.automation.siemens.com/WW/view/de/58246382 With best regards |
1/31/2012 9:59 AM | |
Joined: 4/24/2006 Last visit: 9/26/2024 Posts: 8742 Rating: (1168) |
Hello amitg, Have you seen this link: What to consider when installing WinCC flexible 2008 SP3 or WinCC V11 SP2 on a HP laptop? Best regards, Wizard |
Follow us on