11/21/2017 11:36 PM | |
Joined: 9/27/2006 Last visit: 4/26/2024 Posts: 12257 Rating: (2665) |
Hello Mengo; The TP 177B PN/DP INOX (6AV6642-8BA10-0AA0) was designed for pharmaceutical and food environments, with a higher IP level, a membrane o the screen and an steel bezel: https://mall.industry.siemens.com/mall/en/uk/Catalog/Product/6AV6642-8BA10-0AA0 It appears to be a TP 177B PN/DP (6AV6642-0BA01-1XA1) designed especially for high ingress protection. https://mall.industry.siemens.com/mall/en/ww/Catalog/Product/6AV6642-0BA01-1AX1 I would try to set it up as a standard TP 177B PN/DP, especially if this is only for training purposes. If you need some extra reassurance, you could easily post this questions to Siemens support (there is a link available at the top of this page:Support Request). The Siemens techs will definetely confirm (or not) that you can program the TP 177B INOX as a standard TP 177B. with TIA Portal v14 Professional. Hope this helps, Daniel Chartier |
This contribution was helpful to1 thankful Users |
Follow us on