1/26/2018 10:58 AM | |
Joined: 11/12/2017 Last visit: 2/27/2024 Posts: 174 Rating: (1) |
Hi, quick question I have the power module PM-E 6es7 138-4cb00-0ab0 which is 24v/120v/230v input voltage. Do you have to select the input voltage in the hardware config or is it self selecting? Its just I seen on another power module data sheet you had to select the voltage type (ac/dc). ThanksDavid ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 1/26/2018 2:31:22 PMNew subject after splitting |
|
1/26/2018 12:16 PM | |
Joined: 5/6/2010 Last visit: 9/2/2024 Posts: 1978 Rating: (276) |
Hello DS_7, please look at this link: --deleted Link-- at chapter 10.1 - Parameters for power modules , page 10-2. There you can see the parameters for the configuration of your modul in the hardware config. Hope this is helpful. regards Attachmentmanual_et_200s_12_2004_en.pd.pdf (141 Downloads) |
Last edited by: Jen_Moderator at: 1/26/2018 2:34:05 PMDeleted Link and added file as an attachment. |
|
This contribution was helpful to1 thankful Users |
Follow us on