4/21/2012 5:03 AM | |
Joined: 10/7/2005 Last visit: 5/8/2024 Posts: 3004 Rating: (1046)
|
Hello tarik you have two options: 1.) Use your Step 7 V5.4 and configure the 414-3EM06 (FW V6.x) as a 414-3EM05 (FW V5.x). If you do so, you will miss out on being able to use its new features (e.g. Webserver, I-Device etc.), but it will work and is supported since the 3EM06 is a spare part compatible successor to the 3EM05 (see HERE for more). 2.) Upgrade your Step 7 to V5.5 (this is a chargeable upgrade) and you'll then find the 414-3EM06 in its HWcatalogue and can use all the features it offers. I hope this helps |
Last edited by: fritz at: 4/21/2012 5:05 AMtypos Cheers |
|
This contribution was helpful to1 thankful Users |
4/23/2012 1:30 AM | |
Posts: 71 Rating: (0) |
Hi Fritz, Thank You very much for your help |
This contribution was helpful to1 thankful Users |
Follow us on