4/28/2016 10:14 AM | |
Posts: 5 Rating: (1) |
Same problem for me: I have configured my RIO with TIA Selection Tool, which for Profibus plant with ET200SP (with failsafe) only supplies 6ES7155-6BA00-0CN0. When I try to create the same node in S7 5.5 SP4, I don't have this item and the hardware update only offers me the 6ES7155-6BU00-0CN0. Fafner suggests to use the ...-BA... device, but how can I use it if I don't have it in my hw configuration? Have I to use the ...-BU... card? If it is like this, must I order the BU code or can I configure the BU card in hardware config even if physically there is the BA device? Still don't understand. Can someone explain me? Thanks, Andrea ------------------------------------------------------------------------------------------ |
Last edited by: Blue Moderator at: 4/28/2016 11:36:35 AMNew subject after splitting |
|
Follow us on